Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Occurence Properties Tab

Valued Contributor
Valued Contributor

In the Occurence Property Tab there is an option for "User Defined Quantity". Can we have the default value set at 2 as the minimum.

 

Currently it is one?!

 

Little things... Thanks G

2 REPLIES

Re: Occurence Properties Tab

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't think there's a way to make it conditional. i.e. if there is actually only one make it two. If there are more than two reflect the actual, not two.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Occurence Properties Tab

Phenom
Phenom

If you think about it, having the default as one makes perfect sense.

Why would you ever have a user-defined quantity of one ?

Therefore you know that the required quantity has not been set for that part.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.