Cancel
Showing results for 
Search instead for 
Did you mean: 

Odd file extension shown in display

Experimenter
Experimenter

I've just been uploading some parts into the standard parts library and noticed that the name displayed in Solid Edge is shown with a .par:1 file extension. Any ideas what the reason for for the extra ':1' is? The actual file is just .par as you would expect.

 

SE Filename.jpg

1 REPLY

Re: Odd file extension shown in display

Siemens Phenom Siemens Phenom
Siemens Phenom

You normally see the ":1" after the filename in the tab if you you have the same model open in multiple tabs.  Right click on the tab and select "New Window" to see what I mean.

 

However, I see nothing in your screenshot indicating that you have this file open in multiple tabs.  Without knowing the workflow that got you to this point I would suggest just restarting Solid Edge.