Cancel
Showing results for 
Search instead for 
Did you mean: 

On Off by selction?

Honored Contributor
Honored Contributor

Lets say I graphically select 50 parts of a model. Now those items turn blue in the tree.

 

Is there a way to turn off of the selected items off at one time?

Also: If I selected 50 items in the tree, can I turn all of them on at one time?

3 REPLIES 3

Betreff: On Off by selction?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


no problem!

 

After selection use the RMB and look for "Hide Selected" or "Show selected"

 

Should work for You too!

 

 

PS.: I have put this two functions on my shortcuts menu for keyboard with "Alt+E" and "Alt+A"

which has to do with the German translations for Hide/Show which is "Ausblenden" and "Einblenden"

 

 

regards
Wolfgang

Betreff: On Off by selction?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Forgotten,


and the 3rd one is "Alt+N" for "Show Only" (Nur diesen Einblenden"

 

 

regards
Wolfgang

Re: On Off by selction?

Honored Contributor
Honored Contributor

Good Idea with the hot keys. Just never used that. Most of my models are only 10 to 20 pieces of sheet metal, so I didn't need it. Now things are getting more complicated as I build  up my library of parts.