Cancel
Showing results for 
Search instead for 
Did you mean: 

On the etching of curves when directly developing Orderd Sheet metal.

Creator
Creator

Hello.
Posted after a long absence.


The software used is Solid Edge ST9.


Macsheet of Ordered Sheet metal When developing 3D from direct deployment, etching does not enter dtf file as a line even if curved etching is done. I am going to enter a straight line ....

Would I need to set something?


Thank you.

2 REPLIES

Re: On the etching of curves when directly developing Orderd Sheet metal.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @mo333,

 

You will probably need to go to the drawing view properties, and on the Parts List Options > List All [actually only need to select "List Contructions"], then highlight the [in my example] "Curve Body_1.Etch_1" then check the "Show" box.

 

 

2018-03-02 (3).png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: On the etching of curves when directly developing Orderd Sheet metal.

Creator
Creator

Thank you!

 

In this way I were able to display the curvilinear etching in the 2D drawing a well.

I'm sorry I do not have good English skills.

 

regards