Cancel
Showing results for 
Search instead for 
Did you mean: 

One of the nicest they added to ST8 is?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

I liked to see what people found new and interesting in ST8

 

i love this new "Repair Missing Files" dialog box they've added to assy. Saves time. They need to open also if your accessing the assembly  from draft.

18 REPLIES 18

Re: One of the nicest they added to ST8 is?

Valued Contributor
Valued Contributor

The ability to orient angled planes and the additional handles on dimensions comes to mind.

Re: One of the nicest they added to ST8 is?

Community Manager Community Manager
Community Manager
I personally like the new "top level assembly" filter in the File Open dialog. I am not sure how much production folks would use it, but I am often groping through other peoples stuff and its very handy to be able to pick out the top level ASM by using this filter.
Dan Staples
Director, Solid Edge Product Development

Re: One of the nicest they added to ST8 is?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I like the Compare Drawings tool in ST8.  I tweaked the colors on my system using red and blue to really make the changes stand out.  Very cool addition.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: One of the nicest they added to ST8 is?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

At the risk of sounding far-fetched, I'd say introduction of the "compact" Design Intent panel would do to ST what Walkman did to the music industry. Now everyone's gonna love ST more, use it more, embrace it without hesitation. Time will show - bookmark my post !!

 

Re: One of the nicest they added to ST8 is?

Gears Phenom Gears Phenom
Gears Phenom
Line by midpoint, this is a cool 😎 feature, but assembly contains lots of great features like "variable motor" or "autohide" coordinate system after placing a model and etc... Love this version!

BR,
Imics
http://solidedgest.wordpress.com/

Re: One of the nicest they added to ST8 is?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Looks like they gave us the capability to turn off the Updated Drawing View notification. Which i like a lot. But, how do you turn it back on if needed?

Re: One of the nicest they added to ST8 is?

Valued Contributor
Valued Contributor

Pattern by Table has got to be one of the best new features.  I have used it to the full ability linking the same pattern over 4 parts,  a frame (linked via Project to sketch and a OP set part) , a rubber seal and a 2 part oil pan. All holes lining up perfectly. and any change reflected in all holes. Even links to the pattern of fasterners aswell.  Would be nice to have this option as an assembly feature please #danstaples

 

 

I am finding technical requirements along with the drawing part views linked to assmembly (new in ST7) great, meaning i dont have to check all my callouts and notes every time i make a change.

Consultant - Design Majenta PLM - ST10/MP03

Re: One of the nicest they added to ST8 is?

One thing I can't believe they didn't add was high resolution icons, or any kind of scaling for high DPI displays.

They advertise using the software on a surface pro 3, I can't imagine it's useable on that display. I'm using a 28" 4k desktop monitor and everything is tiny, when I turn on the option for 2x buttons everything becomes pixellated and looks like crap.

Not very impressed.

Re: One of the nicest they added to ST8 is?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Here's a very cool one. Now in the Hole command. once placeing the hole, the next step you no longer have give direction of hole. This will be a BIG time saver

 

somone better not say this is broke...Smiley Happy This is kick butt