Cancel
Showing results for 
Search instead for 
Did you mean: 

Only Seeing .DFT Templates

Experimenter
Experimenter

When I try to open a STEP or IGES or Parasolid, or even just try to start a new file, the only templates that show up to select from are .DFT. All of the other part, assembly and sheet metal templates are in the template folder.

 

Any ideas?

 

Thanks, John

4 REPLIES 4

Betreff: Only Seeing .DFT Templates

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JHighet 

 

 

only just for confirming, You have  a 3D license and not a 2D only?

 

And when set up the template list (from the start screen) You will see all types of templates and not only drafts?

 

 

regards
Wolfgang

Betreff: Only Seeing .DFT Templates

Experimenter
Experimenter

Thanks for the reply Wolfgang. Yes we have the 3D license. One of the other users here was having the same problem and tried running the software as administrator. This solved the issue and the rest of the templates were available. It worked on my computer, too. We don't know why this is necessary, but for now we aren't going to spend time figuring it out. Smiley Happy Just glad to use the rest of the templates.

 

-John

Betreff: Only Seeing .DFT Templates

Gears Phenom Gears Phenom
Gears Phenom

@JHighet   This makes me suspect a virus scan or other sort of Admin security tool.   Make sure to whitelist all SE file types and the SE Install folder. 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: Only Seeing .DFT Templates

Experimenter
Experimenter

Good point @Johnson_BigMatt! Thansk for the tip I'll check that out.  -John