Cancel
Showing results for 
Search instead for 
Did you mean: 

Only outlines lighting up in assemblys

Pioneer
Pioneer

why does only some outlines of my parts are highlighted instead of the entire part, this in the assembly when I glide my cursor over the assembly?

1 REPLY 1

Re: Only outlines lighting up in assemblys

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @KurtCouffez,

 

This looks to be a graphics issue [test by incrementally lowering the setting in SE-Options].......do you have the most current graphics card drivers, and/or are you running Windows10 with the FCU [Fall Creators Update].....if the later is true, then you need to install the update "OS Build:16299.214" as posted about in >this thread here< as it may also help.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000