Cancel
Showing results for 
Search instead for 
Did you mean: 

Open Flash Fit in Assembly

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I have an assembly that requires parts to be relocated. I want to open flash fit to the parts, only get to edit-in-place. 

I've tried setting the part to active then to inactive display nothing happens.

 

What is needed to open flash fit under assembly.

 

Thank you 

Greg

1 REPLY

Re: Open Flash Fit in Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg,

 

Select the desired part [one click only...else will go into edit-in-place mode]..while selected, "Ctrl+select" the existing relationships, then "Delete" them....the click on the "Edit Definition" button that will be floating on-screen....you can now place your NEW part relationships using "Flash Fit" to re-position it. [see video]

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000