Cancel
Showing results for 
Search instead for 
Did you mean: 

Open Save macro available for Insight data?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

I was wondering if anyone using Insight has modified the Open / Save macro so it would work with managed data.  I'm feeling lucky today.

 

Thanks!

Francis

2 REPLIES 2

Re: Open Save macro available for Insight data?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The OpenSave macro supplied with SE in the Custom folder will process Insight files...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Open Save macro available for Insight data?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

My questions is "Why do you want to do this?"

 

We don't recommend to work with it because it is a lot of effort and it changes some information's and you can get "out of date" - drawings

 

Maybe there is another solution for the task you have!

 

Kind regards

 

Stefan

smitsch@unitec.de
www.all4edge.de