Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Open/Save - should it be used?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,



I was asked today wether or not the Open/Save macro should be used nowadays.

 

Is it necessary?

Will it improve the files, performance, the usage of Solid Edge?

Is it a risk to use?

Will data be destroyed?

 

 

So I would like to forward this questions to You with kindly asking You for Your answers, opinion and experience 

 

Thank You very much for all Your response

regards
Wolfgang
1 REPLY 1

Re: Open/Save - should it be used?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello Wolfgang,

in my opinion this macro has its purpose for following scenario:

- User upgrades from very old Solid Edge (V20/ST1 etc.) to actual release (ST10) and wants to use existing data and continue to develop their projects in ST10. Then it is good practise to first "upgrade" old files to curent version of Sold Edge and after that continue to work on files in actual release of Solid Edge.

This aplies for templates also.

 

To give exact answers to your direct questions:

Is it necessary?

Yes, it could be.

Will it improve the files, performance, the usage of Solid Edge?

In my opinion - Yes, if you want to use "very old" files.

Is it a risk to use?

No, I do not think so. I am using it regularly for support customers with transition to newer releases.

Will data be destroyed?

No, in my experience, it never destroyed any files

 

Hope this informations helps you.

 

Ota