Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Open Save

Hi All,

 

We used to use the Solid Edge "Open Save" function, in conjunction with a 3rd party add-in called "Thread Tools"

 

Settings in the Thread Tools program included:

- Hide Sketches & Planes on save

- Update Mass

- Update Drawing Views

- Set to Isometric View

 

Using the Open Save program at the end of a project, provided assurance that the Mass's were up to date, Drawings were all up to date, and we had a nice set of Icons in the windows explorer off all the parts.

 

Unfortunately, Thread Tools has not worked for a few versions, and it now appears that Open Save does not work well in Windows 10.

 

Does anyone have any tips on how to acheive this 'clean-up' outcome, as some of the features of the old style 3rd party programs have been integrated into SE proper over the years.

 

David

 

David Finlay
1 REPLY 1

Re: Open Save

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@trangimagineering, can't answer to the TreadTools, but are you using a saved off version of OpenSave from years ago or are you using the fresh version shipped with ST8/9?  I have not seen issues using the OpenSave shipped wih ST9 on Windows10.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com