Cancel
Showing results for 
Search instead for 
Did you mean: 

Open part in assembly orientation?

Valued Contributor
Valued Contributor

like in SW i can open a part in the same orientation it is in the assembly is there a way to do it in SE.

 

at the moment it opens it in the orientation it was last saved in. 

 

Regards,

MagRiz
(ST9 User Est 01.18)
6 REPLIES 6

Re: Open part in assembly orientation?

Gears Phenom Gears Phenom
Gears Phenom

from the top leave assy you can edit in place into a part and this will show...  but the assy view might still be rotated about the WCS.

 

I think you may be referring to a modeling approach rather than a software command,  but I may be wrong.

 

It seems to me that you are referring to Aerospace or automotive modeling practices where parts are modeled to a similar globally defined WCS.  if this is the case then all parts are "out in space" as related to the WCS...  as the WCS is "assembly based" .

 

You can certainly model this way in SE.  the easiest way is to create a part in place and use the Assy origin for the part origin...

 

 

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7
Highlighted

Re: Open part in assembly orientation?

Community Manager Community Manager
Community Manager

Just double click the part to edit it in context. If you don't want to see the other assembly elements, hit Ctrl Q (hide previous level).

Dan Staples
Director, Solid Edge Product Development

Re: Open part in assembly orientation?

Gears Phenom Gears Phenom
Gears Phenom

@dcstaples wrote:

Just double click the part to edit it in context. If you don't want to see the other assembly elements, hit Ctrl Q (hide previous level).


Funny, it took me 4-5 years before I knew of the Ctrl Q command..  Now it's a programmed button on my space mouse.

-Craig

Re: Open part in assembly orientation?

Valued Contributor
Valued Contributor

oops, i have already reassigned that key stroke to something else. SE didnt warn me it was used for something else.Smiley LOL

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Open part in assembly orientation?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @MagRiz

 

SE does:

 

ControlQHPL.png

Re: Open part in assembly orientation?

Gears Phenom Gears Phenom
Gears Phenom

Hi @dcstaples

 

This command Ctrl+Q is very good, but how to reverse this operation? Is there another Trick?

 

Edited:

 

I've noticed that using Ctrl+Q again, that brings all temporarily hidden parts to be visible.

 

Thank you,

Arek