Cancel
Showing results for 
Search instead for 
Did you mean: 

Opening STP Assemblies Results in Single Body

Experimenter
Experimenter

When I open STP assemblies of customer parts or CAD models of parts I am using for design, they always open as 1 part/body within an assembly. I am choosing assembly templates when prompted, but it still does not split the assembly correctly.

 

When I open these same files in SolidWorks they open as many distinct parts, as they should.

 

I have attached an example below that I downloaded.

 

Thank you.

3 REPLIES 3

Re: Opening STP Assemblies Results in Single Body

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Your step translator settings are probably set to import as a single body part. Turn that off.

 

stptrans.png

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Opening STP Assemblies Results in Single Body

Experimenter
Experimenter

Solved!

 

Thank you bshand.

Re: Opening STP Assemblies Results in Single Body

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That was a quick response! Cool!

That setting should really be in the options dialog IMO.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200