Cancel
Showing results for 
Search instead for 
Did you mean: 

Optimize parts

Legend
Legend

Hi,

 

We have 2000+ parts that have an optimize error  I was wondering if there is a batch or mass tool to solve this error condition.

 

Optimize.jpg

 

Could someone also explain why and when this extra check was introduced and how serious this error is.

 

Kind regards,

 

Jan Bos

Emmen, The Netherlands

User since Solid Edge V3.5 beta testing St10

 

3 REPLIES 3

Re: Optimize parts

Siemens Phenom Siemens Phenom
Siemens Phenom

This is not an error condition per se but is an informational type message.  This need to optimize occurs whenever you import data through STEP, IGES, etc.  We do not do it on import as this will add additional processing overhead and complication to the import workflow.

 

Please see this thread for a detailed explanation of why you should consider optimizing imported geometry:

 

https://community.plm.automation.siemens.com/siemensplm/board/message?board.id=solid-edge-forum&mess...

 

BTW IIRC, Optimize may have came in around ST5….

Re: Optimize parts

Valued Contributor
Valued Contributor

This is not really an error per se.  It is a condition in which an imported solid has not been checked for simplicity.  Many times when a solid is imported from another format you are left with multiple surfaces where there should be one, or multiple edges that can be combined into one.  A good example is a cylinder where the circumfrential surface has been split into two surfaces.  This tool simply performs those simplifications to the model to improve performance.  As far as I know there is no batch tool, and I don't know why this isn't done during the conversion itself.

Re: Optimize parts

Phenom
Phenom

Jan,

 

I use this out of habit on EVERY imported part. As others have mentioned it helps with future editing.... especially if your into Synch. It will find parallel faces, and other Synch type things.  I also usually re-orientate the part so the Synch works too.

 

What I wish they would do is Automate this more.  They should allow for an Import that place the Origin dead smack in the middle of the part so that many faces etc. are ready for editing.

 

Bob