Options.xml

Pioneer
Pioneer

How do you edit this file?  In the past there was a file called SEAdmin.exe used to edit it.  I can not seam to find this file in ST9.

10 REPLIES

Re: Options.xml

Esteemed Contributor
Esteemed Contributor

Hi there @novaman,

 

You'll find "SEAdmin.exe" on the DVD.......browse to the "SptTools" folder.

If you only have the download file, you will need to unpack it to navigate to it.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Options.xml

Honored Contributor
Honored Contributor

... and although it might be clear, but You have to copy it into the SE program folder

 

 



regards
Wolfgang

Re: Options.xml

Legend
Legend

I edit it in notepad, mostly because I haven't installed Gedit or Kate on work machine.


Those who know me question the assigned user rank.

Re: Options.xml

Esteemed Contributor
Esteemed Contributor

@bnemec  I use seadmin to edit options.xml but I've never heard of these editors (gedit and kate). What do you see as their advantages over notepad or, if you know it, notepad++?

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Options.xml

Honored Contributor
Honored Contributor

Hi,

 

 

 

as mentioned by @bshand I also see the SEadmin as the more user friendly tool than any other XML editors.

 

But to complete the list of editors: don't forget the XML Notepad from Microsoft.

This at least is a tool especially made for XML editing

 



regards
Wolfgang

Re: Options.xml

Esteemed Contributor
Esteemed Contributor

I would not advise editing the XML directly using a generic editor.  I've seen some applications crash because of missing tag elements due to accidental deletion or not understanding the XML formatting rules.

 

If you must use a generic editor, I would suggest using one that has XML syntax checking that will warn you when it is malformed.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Options.xml

Pioneer
Pioneer

Thanks for all the suggestions.  I finally found SeAdmin.exe

Re: Options.xml

Pioneer
Pioneer

Thanks for all the suggestions.  I finally found SeAdmin.

Re: Options.xml

Legend
Legend
@bshand they are similar to notepad++ originate from Linux side; I haven't used notepad++ much though. They are handy tools when editing various languages as you can set up color, indenting a couple of spaces instead of tab character etc. for many file types. Much quicker than a full blown IDE for simple stuff. I fear I'm going OT but did not want to be rude and not reply.

Those who know me question the assigned user rank.