Cancel
Showing results for 
Search instead for 
Did you mean: 

Overcome Sync mode

Honored Contributor
Honored Contributor

I have had a rough time trying to use Sync mode. My primary problem is view control.

When I start a sketch in Ordered, the view moves normal to the plane. If I need to rotate to check an include selection, I rotate than use the Control-H command to get back to normal. I can't find how to work the same way in sync mode.

 

And yes I believe my options to be correct, Sync is just different.

 

 

6 REPLIES 6

Re: Overcome Sync mode

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Ctrl+H does not seem to wor in Synch.

I use Ctrl+T, R, L, etc or Look at face to get a view normal to the plane of the sketch.

Re: Overcome Sync mode

Legend
Legend

It works the same way BUT you have to be LOCKED to a specific plane for SE to orient the view accordingly.

 

 

Laurenj.

Re: Overcome Sync mode

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This has been changed in ST7.  Without a plane locked in Synch, the Sketch View command will orient to the most parallel reference plane or if you have started drawing on a part face, it will reorient to that even though it is not locked.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Overcome Sync mode

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Orienting to the closest parallel plane is a nice enhancement.

Hopefully ST7 also orients to the closest isometric view using the QuickView cube.

Re: Overcome Sync mode

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sure does, just click on the corner of the cube closest to you.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Overcome Sync mode

Phenom
Phenom
The QuickView cube is incredibly slick.... just months ago I was complaining about the useless corner orientation triad and what a wasted opportunity it was, and they come up with this visually intuitive little thing that makes my view button shortcuts obsolete!
-Dylan Gondyke