Cancel
Showing results for 
Search instead for 
Did you mean: 

Overide Relationship Problem for a subassembly within another subassembly

Pioneer
Pioneer

Hey Guys,

 

             I just came across this issue.

 

             When i try to override a relationship in a subassembly that particular relationship can't be overriden for other instances of the same subassembly within the main subassembly.

I know its a bit confusing to understand by reading so i am uploading a video.

 

The realtiomship with value 3.31mm is of concern.

I want to move them together with 1 variable table motor

 

Video link: https://youtu.be/DnDDVt-LaYM

 

Any help is appreciated.

 

 

Thanks,

Balaji

5 REPLIES 5

Re: Overide Relationship Problem for a subassembly within another subassembly

Pioneer
Pioneer

hey guys,

 

            Since i dint recieve any replies for almost a week i guess i failed to explain the issue 

            through the video. 

 

            If so please give me feedback so i can upload another video in a bit more detail.

 

Thanks

Balaji

Re: Overide Relationship Problem for a subassembly within another subassembly

Phenom
Phenom

Hi Balaji,

 

As I know, If you are using Adjustable Asseblies you will not be able to override Them.

 

To be able to override them you have to open the Adjustable Assemblies.

 

But if you could furder explain what you are looking for, please do it...

 

Yasser

Re: Overide Relationship Problem for a subassembly within another subassembly

Pioneer
Pioneer

TY for your reply @YD

 

As you can see in the video. I want to overrider relationships in a subassembly(2) which is a part of another subassembly (1). There are 4 subassembly(2) within(inside) the subassembly 1

 

Basically the final goal is to drive them using a variable motor for concept presentation.

 

When i override a particular relationship in a subassembly(2) the same relationship for other subassmebly(2)'s( total 4 nos)  under subassembly(1) disappears because of which i cant drive the other subassemblies (subassembly2) as i cant get them in the variable table and only one subassembly(2) moves.

 

If its still unclear i will try to upload another video.

 

Thanks 

 

Balaji

Re: Overide Relationship Problem for a subassembly within another subassembly

Phenom
Phenom

Sorry Balaji for the delay.

 

If I understand you well, I tried to simulate your situation. I have an Assembly with some Sub-Assemblies. I have to override their relationships to be able drive the Motors.

 

It seems to work. But you could upload a new video if it's possible so that other could contribute to your sollution.

 

Yasser

 

motor_01.jpg

Re: Overide Relationship Problem for a subassembly within another subassembly

Pioneer
Pioneer

Ty for your help @YD

 

Now consider another subassembly withing the subassembly u placed and try to drive that.

 Thats where i am having an issue.

 

I will upload a different video soon.

 

 

 

Thanks,

 

Balaji