Cancel
Showing results for 
Search instead for 
Did you mean: 

Overlapping Assembly Parts

Pioneer
Pioneer

I have a cylinder body with holes in it.  I then bring in shaft ends that partially overlap the existing holes on the main body.  Is there any way that I can desinate the holes take precedence over the shaft ends?  I dont want to modify the shaft ends because they are used in other assemblys as well.  I just want the main bodies existing holes to cut through the shafts where they have intersected.

1 REPLY

Re: Overlapping Assembly Parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI there @JFrost,

 

Could you not use assembly features to do this......assuming that the cylinder can also not be altered, at part level.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000