Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Override diameter prefix in dimension??

Genius
Genius

I have a Inside diameter that I would prefer to have I.D. 5.60 ±0.05 instead of Ø 5.60 ±0.05. I don't see a way to remove Ø symbol in a dimension.

I don't want to use a note as I can't make the tolerance text smaller.

See atached picture, red block is normal dimension, green block is note.

 

Thanks,

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development Emerson Commercial & Residential Solutions | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

3 REPLIES 3

Re: Override diameter prefix in dimension??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Gary_Dinges,

 

You can edit the properties of the dimension [create & save to a style, if you wish to continue using this].....see the "Terminator and Symbol" tab, there is a check box for "Diameter" & "Symmetric Diameter" suppression. Then just use the "Prefix" to add the "I.D." string.

 

 

2017-02-14.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Override diameter prefix in dimension??

Genius
Genius

Thanks Sean, that worked.

Gary

Re: Override diameter prefix in dimension??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

All good buddy!

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000