Cancel
Showing results for 
Search instead for 
Did you mean: 

P&ID Flange Break

Experimenter
Experimenter

I'm trying to do a P&ID in the Solid Edge software.  In the "Connector" annotation selection the only options for start and end are: arrow (hollow, filled and open), slash, back slash, blank, dot, circle and anchor.  I wish there was an option that had a line at the end to represent a flange like the image attached.  Is there an option in there that I am missing?  Does anybody have any other ideas of how to do that?  Thank you.

4 REPLIES 4

Re: P&ID Flange Break

Gears Phenom Gears Phenom
Gears Phenom

@abby1   with the connector command WYSIWYG...  this seems like a valid ER to me.

 

possible workaround?: Have you tried just leaving the end "blank" and placing a block...  

 

not ideal, but 1st thing that came to mind

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: P&ID Flange Break

Experimenter
Experimenter

Thank you for the response @Johnson_BigMatt.  I've actually been using a "flange block" for now as you suggested but also as you said it is not ideal.  I was just hoping there was something that I was missing.  I appreciate you helping.

Re: P&ID Flange Break

Gears Phenom Gears Phenom
Gears Phenom

@abby1   if you all do a lot of P&ID work...  note that with SE 2019 there is a new Modular Plant Design package that is specifically for this sort of work.

 

 

 

 

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: P&ID Flange Break

Experimenter
Experimenter

Thank you @Johnson_BigMatt.  That is good to know.