Cancel
Showing results for 
Search instead for 
Did you mean: 

PART SELECTION

Creator
Creator

HI,

 

IS IT ANY WAY IN SOLIDEDGE LIKE 

WHEN I SELECT PART ITS COLOR CHANGED . 

SEE SCREENSHOT

5 REPLIES

Re: PART SELECTION

Valued Contributor
Valued Contributor

Hi, sometimes I experience this too. I click on a part in the assembly and it is not get highlighted.

Solutions: 

 - If I restart Solid Edge it usually helps .

 - Maybe update your graphic card driver.

 - Empty windows TEMP folder.  Close all windows, then enter this in the windows Explorer : %temp% and delete all files and folders (the system won't allow to delete some, so just skip them when prompted)

 

Re: PART SELECTION

Creator
Creator
DONE ALL THAT STEPS
BUT NO RESULTS
MY GRAPHICS CARD DRIVERS IS UP TO DATE.

Re: PART SELECTION

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Since you've been using Solid Edge has it always behaved as you show in the photo? If so, I think there's an issue with your system. I've tried changing settings to make my system not highlight the part like yours and I can't do it. It always highlights, depending on my settings, either with a glow, or just the edges highlight.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: PART SELECTION

Gears Phenom Gears Phenom
Gears Phenom

Hi @Raumik

 

try to play with your settings :

 

settings.png

 

regards,

 

Arek

Re: PART SELECTION

Siemens Phenom Siemens Phenom
Siemens Phenom

Try changing the selected color:

 

Application Button -> Settings -> Options -> Colors -> Selected