Cancel
Showing results for 
Search instead for 
Did you mean: 

PC specs for Solid Edge

Creator
Creator

Hi all

 

just thought I would share my PC specs as I've seen a few people with SE speed issues.

 

I recently added more RAM to my self assembled machine and it's running ST9 MP03 without any major trouble. Before I added more RAM it was beginning to slow down in a medium sized assembly (255 total parts, 42 unique parts, 6 simplified parts, 3 levels, 10 subassemblies, 5 unique subassemblies, 140.62MB)

 

Intel NUC Mini PC Kit NUC6I5SYH A$599

fitted with

Intel 540s Series 240GB SSD, m.2(SATA) A$119

1x Kingston KVR21S15S8/8 8GB (1x8GB) 2133MHz DDR4 SODIMM A$69

1x Kingston KVR21S15D8/16 16GB (1x16GB) 2133MHz DDR4 SODIMM A$135

 

that's it

 

the PC kit has the same graphics engine as a Microsoft Surface Pro 4 i7 and the processor from the i5.

 

one tip with this setup is to keep the graphics driver up to date manually, the automatic driver update doesn't always do the job.

 

I've also witnessed a speed improvement when updating my monitor, I'm now using a BENQ EW2775ZH A$329

 

Is this the cheapest SE CAD workstation in the world?

 

Tony

www.mazcad.com

Edging since V18
4 REPLIES 4

Re: PC specs for Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Awesome info Tony [ @MazCAD ].....imagine if it were aslo a touchscreen monitor. [almost a Surface Studio Robot wink ]

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: PC specs for Solid Edge

Creator
Creator

Smiley Happy

 

I think my arms would get tired

 

But I am wondering when we will see SE on an Occulus Rift...

 

 

Edging since V18
Highlighted

Re: PC specs for Solid Edge

Genius
Genius

Whauw, that's interesting !

 

Can you tell me a bit more about your configuration setup.

Can you add 3 monitors to it ? And does the GPU have enough power to support them.

 

Is it your daily used Solid Edge workstation or just testing for fun ?

What's the largest asm you have opened with this Intel NUC.

 

Anyway it would be a great replacement for a LARGE and HEAVY desktop i think in the future

if they also produce mini pc's with pro GPU's in it.

And better would be that I simply grap my smartphone in the morning with solid Edge running on it.

And nothing more ! bye bye desktop,notebook and tablet.

So I guess I will be seeing this before I go on pension Smiley Happy

Dirk Rutten

Solid Edge ST6 user !!!!

Re: PC specs for Solid Edge

Creator
Creator

here's a link to the Intel page with specifications

http://www.intel.com.au/content/www/au/en/nuc/nuc-kit-nuc6i5syh.html

 

it has two video outputs, 1x full-size HDMI & 1x mini displayport

 

here are the assembly stats for the largest assembly I have

 

Capture.JPG

 

here's a video of it in action

 

it's a bit jumpy when zooming because I'm using a mouse wheel

http://mazcad.com/intel-nuc-3d-mechanical-cad-demo-large-assembly/

 

there's also a video of a zoom operation using a 3D controller

 

Edging since V18