Cancel
Showing results for 
Search instead for 
Did you mean: 

PDF 3D options

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Is there a way to set the background color of the 3D PDF or to assign a template (to include the company's logo, for instance)?

 

TIA

7 REPLIES

Re: PDF 3D options

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Doesn't it take the background of the SE 3D view style settings?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: PDF 3D options

Pioneer
Pioneer

There may be a way to set the background I just haven't found it yet; as for templates, if you're using Adobe Reader I think you're somewhat limited in what you can do - although the new Reader DC may have some ability, but if you have Adobe Acrobat you can create templates that include your company's logo and other relevent data.

 

Dave

Re: PDF 3D options

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

It is what it is!

There are no options available to customize the layout.

 

The only way to do this is with additional solutions.

Samples here:

http://www.all4edge.de/uploads/media/PowerPack_01.pdf

http://www.all4edge.de/uploads/media/Grinder1.pdf

 

http://www.all4edge.de/produkte/3d-pdf/beispielebestellung/

 

Videos:

Compare

http://www.youtube.com/v/KvYOi-T3BvE

 

How it works

http://www.youtube.com/v/ljyWg2ZvSq4

 

Stefan

smitsch@unitec.de
www.all4edge.de

Re: PDF 3D options

Valued Contributor
Valued Contributor

I tried saving 2 simple parts as 3D PDFs, but all I get are blank PDFs.  Is there anything I need to do other than click on Save As - Save As Translated and pick 3D PDF as the file type?

Re: PDF 3D options

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@SPXAli wrote:

I tried saving 2 simple parts as 3D PDFs, but all I get are blank PDFs.  Is there anything I need to do other than click on Save As - Save As Translated and pick 3D PDF as the file type?


Hi there,

 

Make sure you're using Adobe Reader to open the files.....not the "reader" for Windows 8.

[right click on the PDF choose "Open With", select Adobe Reader]

 

Windows8_3D-PDF_OpenWithAdobeReader.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: PDF 3D options

Pioneer
Pioneer

It's pretty straight forward in that you have some control over the amount of detail you want in the finished product.

 

What version of Adobe Reader or Acrobat are you using to view the PDFs?

 

Re: PDF 3D options

Valued Contributor
Valued Contributor

Thank you.  I was using Nuance Power PDF to open it.