Cancel
Showing results for 
Search instead for 
Did you mean: 

PIPING APPLICATION

Creator
Creator
Piping module
Hello,
I can not install, halfway on a line of piping, 1 valve + 2 gaskets + 2 flanges, with no space between each.
Here is my procedure:
- I cut the line of my sketch to all the places where I want my components.
- Unfortunately I can not control the distances between each of them.
- When I click on the intermediate insertion points, to insert a flange for example, the Standard Parts dialog box does not propose the category of flanges or gaskets.
All these components are installed in the SE library.
Do I have the right method or what?
In the videos available on Youtube or other sites, we can see on their general 3D valves and accessories. However we do not see the work procedures to get there.
Thank you
1 REPLY 1

Betreff: PIPING APPLICATION

Legend
Legend

Hello,

 

The piping tool you use is in solid edge is xpresroute or smap3d?

Alternatively, do you create a path as example with frame, 3d sketch or 2d sketch?

Use you direct the standard parts.

If you use a flange connection, you need a gasket between it too.

If you use xpresroute have you try defining all fittings you need?

 

best regards

Wolfgang