Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI Baloons in the Assembly

Experimenter
Experimenter
Hello,

-In the draft I know that the balloons are interconnected with the parts list.
-But in the assembly in PMI> Annotation> Ballon, you have the option to insert the balloons, you can enter a value manually or call a link from somewhere I do not know where it is .......
-Does anyone know how this option is linked?

Sem título.png

Renan Dornelles.
3 REPLIES

Betreff: PMI Baloons in the Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @RenanTche

 

 

there is only one issue I can imagine that You haven't done so far.

 

Have You set the assembly options to keep position numbers in 3D file (see picture)

 

I have done so nad You see the result on the right, that PMI balloons show assembly pos numbers

 

20161125_1516.PNG

 

Before activating this option there was a n/a (not available) in the balloon text field

 

 



regards
Wolfgang

Betreff: PMI Baloons in the Assembly

Experimenter
Experimenter
Hello wolfgang

Many thanks friend, you helped me a lot !!!
God bless you.

Renan Dornelles

Betreff: PMI Baloons in the Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Welcome and thanks

 



regards
Wolfgang