Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Edger´s

 

I have an strange behaviour. I have an SE Part with PMI´s.

 

  1.  Export this .par as JT
  2. Import again in Solid Edge
  3. The PMI´s are imported as Annotation....

Is this an issue only at my Installation or has someone the same Issues?

 

ST9 MP4

 

2017-01-27 10_01_14-Solid Edge ST9 - Sequentielles Teil - [000-015-937.par_1].pngSolid Edge .par2017-01-27 10_02_37-PathFinder.pngJT importes from .par2017-01-27 10_03_40-Speichern unter.pngJT Options

9 REPLIES 9

Betreff: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
One Note i have forgotten: It is not related to sync or seq the result is the same

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

on my W10 machine and ST9 MP4 import from JT with PMI regenerates true PMI dimensions. I used same and different JT settings.

So I can not confirm your issue.

 

Ota

Highlighted

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Could you share a model?

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Here is on of the model´s

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Thx Ota for ur answer, i will check if it is an issue with the model...

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Edger´s

 

I think i have figure it out, it is related to the Dimension Type "Symmetric Diameter"....

 

Could you please confirm me this, than i will file an IR.

 

THX a lot in advance

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

I tried export and import as JT your model. I got PMI dimensions as annotations.

But when I created my simple model and exported and imported from JT, I got PMI as PMI dimension.

Try my file and let me know.

Maybe next interesting fact is that your file was created in version Solid Edge v10. Maybe this issue can be related to this because I had another issue with thread extend in hole feature in files created in SEv17.

 

Ota

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Ota,

 

yes you are right it works also for me. I added one Dimension and you will se this does not work....

 

 

I filed an IR and it got an PR 7943732

 

Thx for helping me to figure this out edger´s

Re: PMI Dimensions are exported to the PMI as Annotation ST9 MP4

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

PMI can be "Semantic" & "Polyline" object. Polyline is used in viewers and it is a representation mode. Solid Edge ST7 was the first version which supported export/import PMI. In Solid Edge the "Symbolic" utilizes the Polyline representation of the PMI. Symmetric, ballons, dual dimensions will be represented as symbolic, but they will not be attached to any edges or vertex...

 

The new JT translator (ST10) can be provided more as @ota_poul2 has already mentioned.

 

BR,

Imics
http://solidedgest.wordpress.com/