Cancel
Showing results for 
Search instead for 
Did you mean: 

PMI balloon in ASM using API

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


after trying without any positive result I must ask wether anybody has a hint or an idea how to create a PMI balloon in an assembly via API

 

What I want do achioeve is to run through all occurences (top occurences) witihn an assembly and create a PMI balloon with occurency name and postion connected to them.

 

I have seen that thee is a SEApp.ActiveDocument.PMI section holding the balloons in it.

 

Using ...balloons.addByTerminator(object, dblX, dblY, dblZ, keypoint) didn't bring me to a proper result

 

Thanks in advance for any hint and tip or code 

 

regards
Wolfgang
2 REPLIES 2

Re: PMI balloon in ASM using API

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Isn't this more of a developer forum question?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: PMI balloon in ASM using API

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


Yes, I have put it now into the developers forum.

 

Thought, since here are online so many programers I will give it a try here.

 

Sorry

regards
Wolfgang