Cancel
Showing results for 
Search instead for 
Did you mean: 

PROBLEM DURING CONVERTING TO DWG

Creator
Creator

when i made any drawing in solid edge draft in colored lines, and converting it into DWG file then the colors of all lines became white, instead of keep in colored. what should i do to convert the lines in same colors as it is in solid edge

 

5 REPLIES

Re: PROBLEM DURING CONVERTING TO DWG

Phenom
Phenom

Hi Rahul,

during opening a DWG file you have to clock on OPTIONS and make some changes to get the desired result concerning the colors of your lines.

 

Yasser

 

dwg_options_02.jpg

Re: PROBLEM DURING CONVERTING TO DWG

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

My understanding of the question is Rahul wants to save the Solid Edge drawing to .DWG and wants to see the colors used from SE in the DWG. If yes, I am able to verify this.

  

My best guess and workaround is if the drawing elements are organised on layers in Solid Edge, then the Options wizard in DWG SaveAs dialog has a facility to map color based on layers.

This worked for me and that's the closest I am able to get based on my limited knowledge in this area.

  

~Tushar Suradkar

 

P.S.

1. This might involve some-rework and re-organization but CAD standards are always useful.

2. Nice to see someone doing some serious AEC stuff in SE Drafting Smiley Happy

 

Re: PROBLEM DURING CONVERTING TO DWG

Creator
Creator
Thank u so much sir. I'll try it

Re: PROBLEM DURING CONVERTING TO DWG

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

As @Tushar says...in the DWG save "Options" area, there is a check box that makes this all work like you need it to.....uncheck the "Do Width to Color Mapping" box, and click finish.

 

2015-11-17.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: PROBLEM DURING CONVERTING TO DWG

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

You will want to be looking at you SEACAD file. The wizard can be accessed by selecting save as DWG, then click options. Depending on how the colours were generated, and how you would like to present your drawing, you can either assign colours and linetypes to layers, or colour width mapping.

Shane Murray
ST10 MP8