Cancel
Showing results for 
Search instead for 
Did you mean: 

PacEdge - Free Pack and Go for Solid Edge

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello everyone,

 

I am glad to introduce PacEdge - a free Pack and Go program for Solid Edge.

 

The program is open source. A detailed tutorial on how to build this program from scratch also exists and can be read here.

 

This is an attempt to make a Solid Edge version of similar programs in SW and Inventor but in no ways an alternative to the powerful and feature rich Revision Manager.

 

The program executable can be downlaoded only at the end of the aforesaid programing tutorial. So you may need to browse through the pages till the end.

Here's a preview of version 1.0 of the program:

 

01.png

 

~Tushar Suradkar

www.SurfAndCode.in

 

11 REPLIES 11

Re: PacEdge - Free Pack and Go for Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Awesome @Tushar.....now just to get THIS integrated into Solid Edge ST8.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: PacEdge - Free Pack and Go for Solid Edge

Gears Phenom Gears Phenom
Gears Phenom

There in no word for this my friend!

 

mt.png

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: PacEdge - Free Pack and Go for Solid Edge

Phenom
Phenom

Excellent work!!!

-Dylan Gondyke

Re: PacEdge - Free Pack and Go for Solid Edge

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Thanks Tushar!

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: PacEdge - Free Pack and Go for Solid Edge

Phenom
Phenom

This should definitely make an appearance in the Custom Directory in ST8.

-Dylan Gondyke

Re: PacEdge - Free Pack and Go for Solid Edge

Valued Contributor
Valued Contributor
Downloaded the exe from your site @Tushar but the program fails to run. I'm running ST8. Dose it need to reside somewhere specific?

Thanks,
Guy

CAD/CAE Manager
SE2019 MP5

Re: PacEdge - Free Pack and Go for Solid Edge

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@Guy_H77 I can also see the one from my site is not working.

Can you kindly check if the attached version is working ?

Thanks for reporting.

   

Tushar

Re: PacEdge - Free Pack and Go for Solid Edge

Valued Contributor
Valued Contributor

@Tushar thanks for the upload, unfortunately I get the same issue.  I've placed the folder in the ST8 cutom folder and added an exception to my antivirus.

 

 2017-06-23 09_13_01-PackEdge (1).jpg

 

Guy


CAD/CAE Manager
SE2019 MP5

Re: PacEdge - Free Pack and Go for Solid Edge

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Do you use Visual Studio or know someone who can build the program from the source code.

I can share the VB.Net project files.

  

~Tushar