Cancel
Showing results for 
Search instead for 
Did you mean: 

Pack and Go in Solid Edge?

Builder
Builder

Again coming from solidworks, I used its Pack and Go function very often. Was wondering if Solid Edge has an equivalent command?  

18 REPLIES 18

Re: Pack and Go in Solid Edge?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

what is it?

Re: Pack and Go in Solid Edge?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is not anything delivered with Solid Edge that provides the same functionality, but you can replicate it with Revision Manager by copying the structure to a new folder and performing a "where used" for the Drafts and copying them as well, then zip the folder and send.\

 

Alternatively, a company called Hitteam has a product that aims to provide the same functionality as Pach and Go:  http://hitteamtools.com/activePach2Go.html

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Pack and Go in Solid Edge?

Builder
Builder

Thanks Grundey. I will most likey try your sugestion later this week. Have you used the Hitteam tools download?

 

TDB, Solidworks' Pack and Go is a command that, "Gathers all related files for a model design (parts, assemblies, drawings, references, design tables, Design Binder content, decals, appearances, and scenes, and SolidWorks Simulation results) into a folder or zip file." Dassult Systemes.

Basically its really nice for when you need to create an assembly that is similar to an extisting assembly and you just need to change a few dimensions or components. For example, I used this alot designing cabinets when I needed a different width or depth version or what I had already drawn. 

Re: Pack and Go in Solid Edge?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have not used their tool.  We rarely send stuff out and when we do, we just use Revision Manager to do it.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Pack and Go in Solid Edge?

Community Manager Community Manager
Community Manager

@SW for what you are doing, Revision Manager will actually be better than Pack and Go. You pick the top level ASM to "clone" but then throughout the structure you can define for each part whether to leave it alone (continue to reference existing) or copy it to a new name or revise it. It takes a few swings to get the hang of it, but once you do, you'll find it indispensible. 

Dan Staples
Director, Solid Edge Product Development

Re: Pack and Go in Solid Edge?

Siemens Genius Siemens Genius
Siemens Genius

Hello SW:

 

Here is a way to do it using Revision Manager:

 

1) Open the top-level assembly in Revision Manager.

2) Click in the upper-left-hand corner of the table of the structure to highlight all rows of the assembly.

3) Right click on the highlighted rows and choose "Set action to copy" from the context menu.

 

Notice that the action has changed to "Copy". 

 

4) With all rows still highlighted, choose Home -> Action -> Set Path. 

 

This will allow you to define a new path for all highlighted entries. 

You may also assign new file names if you wish.

 

5) Choose Tools -> Where Used and provide the location where to locate the drawings of all items.  This is probably in the same location as the components themselves.

6) Click Next, then Finish.

 

Notice in the bottom pane we now list all the files from the top pane - and if you expand them out you will see the drawings associated with them.

 

Hold down Control and click on the box to the left of each drawing you wish to copy.  This highlights them.

 

7) Right-click on the highlighted items and choose "Set action to copy" from the context menu.

8) While they are still highlighted, choose Home -> Action -> Set Path and set a path for the drawings.

 

Steve

 

* My opinions are my own.

 

 

 

Steven Sheldon
Advanced Applications Engineer
Siemens PLM Software

* Opinions expressed are my own.

Re: Pack and Go in Solid Edge?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Another alternative is PacEdge - a Pack and Go program for Solid Edge. A detailed tutorial on how to build this program from scratch also exists and can be read here.

 

I have tried to make it look as much as the one in SW, though also note that this is not a replacement for Revision Manager. Infact it is based entirely on the RevMgr API.

 

Using the free source code, you can build your own version of Pack n Go for Solid Edge.

Here's a preview of version 1.0 of the program:

 

01.png

 

~Tushar Suradkar

www.SurfAndCode.in

 

Re: Pack and Go in Solid Edge?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Awesome @Tushar.....now just to get THIS integrated into Solid Edge ST8.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Pack and Go in Solid Edge?

Phenom
Phenom

RM works, but when you have an assembly spread over several maps and (OK, not wright) you have parts named the same over severall maps you can't use RM.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user