Cancel
Showing results for 
Search instead for 
Did you mean: 

Parallel Mates?

Pioneer
Pioneer

I'm trying to create a parrallel face mate, a pretty easy task in Solidworks that I use a lot as I'm creating assemblies. In SolidEdge I only seem to be able to select an edge, and then it doesn't make them parallel, it connects them. I don't see any menu for selecting a face instead of an edge or anything like that. 

 

Any suggestions?

 

Thanks.

14 REPLIES

Re: Parallel Mates?

Gears Phenom Gears Phenom
Gears Phenom

I don't know if I understand your question correct, but I think you are looking for a floating mate, no?

 

click on:

klik.png

 

choose: 

mate.png

...........................................................................................................
Solid Edge ST10 & AutoCAD 2019 user

Re: Parallel Mates?

Gears Phenom Gears Phenom
Gears Phenom

Are you referring to a planar align?

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Parallel Mates?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes, Planar Align or Mate is what you are after.  The Parallel relationship is for edge to edge contact.  Planar Align and the Mate will do what you want, but be aware that these look like they do the same thing (make two faces parellel with either a floating or fixed offset) but they have one major difference.  Mate orients the face normals (imaginary perpendicular vector on the face pointing away from the solid) in opposite directions and the Planar Align points them in the same direction.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Parallel Mates?

Gears Phenom Gears Phenom
Gears Phenom

As Ken mentioned if you think of it as a bookcase, the mate puts the books side by side and the planar align aligns their bindings.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Parallel Mates?

Pioneer
Pioneer

Thanks, but I'm not sure I want either of those. I want the two faces to be aligned with each other, but not to constrain the distance or anything else. Imagine you're building a cad sandwich, you want the faces of the two slices of bread to be be parallel, but not define the distance or location in space. 

 

When I do a Planar Align it puts them on the same plane, not what I want, I just want them parallel. 

Re: Parallel Mates?

Gears Phenom Gears Phenom
Gears Phenom

You need planar align, but click on the ruler (this is for fixed distance) and choos the blue arrows. Than the faces will be aligned without a fixed distance. (see screenshot in my first post)

...........................................................................................................
Solid Edge ST10 & AutoCAD 2019 user

Re: Parallel Mates?

Pioneer
Pioneer

Hi Joris, thanks, that wasn't working but then started working, maybe something to do with mates not updating until I move things around?? When I 'turn off' (uncheck in the tree) a part in an assembly, does that not stop the mates associated with that part from constraining another part? 

 

I've noticed that Rigid and Adjustable Assembly are greyed out in my version. Do you know if I perhaps have some other setting that is causing that, or just due to the version I have (Design 1)? Currently I'm rebuilding the assembly with no sub-assemblies (not something I'm a fan of).

 

btw what is the proper process for eliminating a mate? I've been highlighting the part, click Assemble, scroll to the mate I want to eliminate, which is then visible in the small window but it's not highlighted so I can't delete it, so I select it again but that just shows all the mates again, so I have to highlight it again, then I can delete it. I'm guessing there's a better way?

 

Also is there a way to temporarily deactivate/activate a mate?

 

Thanks.

Re: Parallel Mates?

Gears Phenom Gears Phenom
Gears Phenom

When you 'turn off' a part, (luckily) the constrains stay.

When you want to suppres a constrain, RMB click on the constrain an click Suppress

 

Eliminate a constrain:

Click on a part

RMB click on the constrain

Deleta relationschip

 

or

click on the part

click (left mouse button) on the constrain

hit the Delete button

 

...........................................................................................................
Solid Edge ST10 & AutoCAD 2019 user

Re: Parallel Mates?

Honored Contributor
Honored Contributor

I have been wondering what the differance between mate and planar are. My mate'sm are almost always are backwards and I typically use mate. I will now switch to using planer align. Maby I won't have to flip everything now. I will likly still end up with negative offset values most of the time!