Cancel
Showing results for 
Search instead for 
Did you mean: 

Parametric File Properties, Occurrence Properties

Valued Contributor
Valued Contributor

Hello,

 

Is there any way to paste excel link in cellls of File Properties dialog box like "Project Name' or 'Document Number'?

Is there any way to to paste excel link in cellls of Occurence Properties dialog box like 'User Defined Quantity'?

 

Or is there any other way to get similar results?

 

Regards,

Aslam

3 REPLIES 3

Re: Parametric File Properties, Occurrence Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Excel cells can only be linked with variables in the Variable Table, however a variable can be exposed as a Custom Property and then consumed via Property Text.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Parametric File Properties, Occurrence Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

AFAIK a link from Excel to Solid Edge variable table only is possible using numeric values but not for text properties.

 

So IMHO this might not be the solution for @aslam

 

But the better question will be why will Excel to Solid Edge the better solution than keeping it internally?

 

I have heard that much often "we need an Excel table"  to connect it to Solid Edge where on the other hand the internal function are at least as good as the external ones but they will be inside, associative and faster than any external.

 

And if it is conerning textual properties, Excel anyway will be unable to use.

 

 

regards
Wolfgang

Re: Parametric File Properties, Occurrence Properties

Valued Contributor
Valued Contributor
Hi hawcad and Kenny G

Thank you for your comments.

Regards,
Aslam