Cancel
Showing results for 
Search instead for 
Did you mean: 

Parametric control of layers.

Not applicable

Is it possible to have a boolean variable to control whether the layers are turned
on or off?
I'd like to display something on some drawing sheets but not on others.
If I could turn a layer on or off I could then have the feature on that layer and
have it linked to the excel files with a 1/0 True/False on/off variable to switch
it.
-AS
www.continual-motion.com
2 REPLIES

Re: Parametric control of layers.

Not applicable
Andy,
With the Free 2D Drafting software this is not possible. The properties of
objects, such as show/hide of layers, are not exposed. The applications
interface that you would use to write your own macros to control this is
disabled. You need full Solid Edge to accomplish this.
Regards,
Rick B.

Re: Parametric control of layers.

Not applicable

Pity there is no way of doing this!
"Ricky Black" wrote:
>Andy,
>With the Free 2D Drafting software this is not possible. The properties of
>
>objects, such as show/hide of layers, are not exposed. The applications
>interface that you would use to write your own macros to control this is
>disabled. You need full Solid Edge to accomplish this.
>
>Regards,
>Rick B.
>
>

www.continual-motion.com