Cancel
Showing results for 
Search instead for 
Did you mean: 

Parent lost sketch..

Valued Contributor
Valued Contributor

Hi edge users ..

Sketch extracted with inclusion lost parent.
Can I use this line only by using it?

Line0.png

How do I fix the blue dimensions so that I can control them?

 

5 REPLIES 5

Re: Parent lost sketch..

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Hclee,

 

You could just delete the "links"...and re-assign the profiles missing plane, to the nearest one.

Is the attached OK....?

 

 

Oh, I see your edited post.......so the dimensions, I just clicked the "lock" toggle icon to make them driving.

 

2016-11-23 (3).png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Parent lost sketch..

Valued Contributor
Valued Contributor

Thank you.
Where do I delete links?

Re: Parent lost sketch..

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Hclee wrote:

Thank you.
Where do I delete links?


Welcome. 

Edit the sketch profile, Ctrl+select the chain icons...delete on keyboard.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Parent lost sketch..

Valued Contributor
Valued Contributor

Aha!
You can delete the constraint.
Thank you.

Re: Parent lost sketch..

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

 

every relation in sketch is an object as any line or circle and so not only can be created but also can be deleted.

Sometimes Your requests concerning Your sketch or further the 3D model will be change and so it is important that You can change Your definitions as Your requests will change.

 

 

 

regards
Wolfgang