Cancel
Showing results for 
Search instead for 
Did you mean: 

Part Copy Reference

Creator
Creator

We use part copy on some of our models.  We have some base parts and some different core that can mix and match to create differnt parts.  We bring in part copy(1) then part copy(2) then subract part 2 from part 1.  Is there a way to reference the copied part in the draft.  Can I create a note or callout that is tied back to the copied parts?  We don't really want to create a parts list, just a note that we can reference back to the original copied parts.

JD Haigler
2 REPLIES

Re: Part Copy Reference

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No, there is no way to get the info of the Part Copy from Draft.  You can however use an assembly file to position your parts and then boolean one or more from a target part, and then you can use the assembly for the "mixed" part.  Just set your occurence properties for your "tools" to not show when placed in an assembly.  You will want them for drawings in order to pull their properties.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Betreff: Part Copy Reference

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi 

 

as mentioned by @KennyG there is no direct metjod to accomplish what YOu want.

 

But I think it could work to ceate a property within the part showing which references are used.

This should not be a big problem for a small macro.

And this property can be used in drft or whereever it might be necessary

 

What do You think about this idea?

 



regards
Wolfgang