Part List rearrange issue

Legend
Legend

Hello,

 

I am having the issue with a rearranging the list in the Part List.

I have found a few topics regarding to this problem.

But, i cant change the list manually in the Data Tab.

 

part list.png

The buttons on the left are inactivated unfortunatelly,

 

Thank you for help.

 

Regards,

 

Arek


Production: SE ST10 MP3
;
7 REPLIES

Re: Part List rearrange issue

Phenom
Phenom

You will need to set the sort option to 'blank', then you can use the move up/down.

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.

Re: Part List rearrange issue

What platform do you use? ST X ? With or Without Teamcenter?

Ciprian Chiosa
Solid Edge ST8 + TC10.1 - Win 7 x64
SIPA Enginnering Romania

Re: Part List rearrange issue

Honored Contributor
Honored Contributor

In general you have to either use the sorting, or manually number every part. Making a single change to what you have is not possible.

Re: Part List rearrange issue

Esteemed Contributor
Esteemed Contributor

@12GAGE, You, for some reason, are not accepting of the fact that you can use the data tab to rearrange parts lists.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Part List rearrange issue

Honored Contributor
Honored Contributor

You are right. I exclude using that for a reason and forgot that it was even possible.

 

I frequently have a bom on one page with bubbles pointing too a small view of the assembly.

 

Then on the next page, same thing, but the BOM is off the page for a larger view of the assembly (I work on A size paper)

 

If I were to use that funtion, I could really have a mess on my hand. 

 

So in this case, my peronal proceudres made me think about the question wrong.

 

Thanks!

Re: Part List rearrange issue

Esteemed Contributor
Esteemed Contributor

If I were to use that funtion, I could really have a mess on my hand.


I don't get why. It's all easily reversible.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Part List rearrange issue

Honored Contributor
Honored Contributor

I would have to edit two cases of the same BOM in some cases. For frame members, I sometime use items number to track the part. This would become something else to check that I don't want to check. I have to produce drawings to quickly. I use procedures that minimize the checking I need to do.