05-15-2014 08:18 AM - edited
I noticed in part painter the colors are basically the same plain colors. I looked in Color Management> color in the SE, Property Management> Material Table> In this table I do see adjustment modify for face and fill> on parts not text. Cannot find an adjustment for part painter. I would like to change colors in the text.
Thank You
Greg
Solved! Go to Solution.
05-15-2014 09:27 AM
Greg, that works differently than the face style setup. Just start the Text command, click the Color button on the command bar, and then select More... It will open a color pallette which will allow you to create any color you want and then "Add to custom colors" for repeated use. Just a reminder that this is stored in that file only so if you want these in all files, set them up in your template file.