Cancel
Showing results for 
Search instead for 
Did you mean: 

Part Painter Readjust In Solid Edge

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I noticed in part painter the colors are basically the same plain colors. I looked in Color Management> color in the SE, Property Management> Material Table> In this table I do see adjustment modify for face and fill> on parts not text. Cannot find an adjustment for part painter. I would like to change colors in the text.

 

Thank You

Greg

1 REPLY

Re: Part Painter Readjust In Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg, that works differently than the face style setup.  Just start the Text command, click the Color button on the command bar, and then select More... It will open a color pallette which will allow you to create any color you want and then "Add to custom colors" for repeated use.  Just a reminder that this is stored in that file only so if you want these in all files, set them up in your template file.

 

color.png

 

 



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com