Cancel
Showing results for 
Search instead for 
Did you mean: 

Part copy- ST8 MP9, where's material link?

Legend
Legend

I don't see the choice to link material when doing a part copy now. Anyone else notice this, or did it move somewhere with the latest maintenance pack? I now have the choice to copy colors..............Smiley Sad

 

 

ST8 MP9
Go FAST, or go home.
7 REPLIES 7

Re: Part copy- ST8 MP9, where's material link?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I see it so it must be MP9.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Part copy- ST8 MP9, where's material link?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Part Copy must be placed in the Ordered environment (no associativity in Synch...) and it must also be the Base Feature (if other bodies already exist in the file then the option is not available).



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Part copy- ST8 MP9, where's material link?

Legend
Legend

That's the way I use it, but I don't see the button to activate linking material now that I'm on ST8 MP9. I looked again, must be something with the base feature. I'll do more investigating.

 

Thanks!

ST8 MP9
Go FAST, or go home.

Re: Part copy- ST8 MP9, where's material link?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We're on ST9 now, but, it appears to be functioning as expected.....

 

ST9_PAR_Ordered_IPC_PartCopyParameters.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Part copy- ST8 MP9, where's material link?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Grundey wrote:

Part Copy must be placed in the Ordered environment (no associativity in Synch...) and it must also be the Base Feature (if other bodies already exist in the file then the option is not available).


You still get the link material button in synch but not link file.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Part copy- ST8 MP9, where's material link?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's there is Synch, but since there is no associativity it does not actually "Link" the material, it is just copied at the time the Part Copy is created.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Part copy- ST8 MP9, where's material link?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That wasn't really the question I don't think, but, yep, of course.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200