Cancel
Showing results for 
Search instead for 
Did you mean: 

Part exist in a assembly without existance in a tree

Experimenter
Experimenter

I was working on a assembly which is showing the part in a pattern but it is not reflecting its presence in a assembly tree.

This part is not even showing the delete option.

When I have changed the verical pipe length, then this part becomes unsymmetric. 

It would be really helpful if anyone suggest, how to tackle this error.

 

 

 

 

 

5 REPLIES

Re: Part exist in a assembly without existance in a tree

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think there may not be enough information to understand the problem you are having.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Part exist in a assembly without existance in a tree

Experimenter
Experimenter

Mr. bshand,

 

It would be really helpful, if you let me know what other information you are looking for?

 

Re: Part exist in a assembly without existance in a tree

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Rahul:

 

What @bshand perhaps means is the information you provided and the images are not enough to fully understand your problem.

In Image1, you have selected Pattern 4 in the Pathfinder and a green part is highlighted.

You cannot right-click on an individual part of a pattern to delete.

For deleting a pattern right-click on it in the PathFinder tree.

To remove a single instance in a pattern uncheck it in the Pathfinder

 

Hope this helps solving some of your issues.

 

Further you said " how to tackle this error."

Where is the error message, post a screenshot of the error.

 

Please make efforts to make your question clear and obvious to the reader.

 

Best wishes,

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group

[ Everything under the Sun about - Solid Edge ]

 

Re: Part exist in a assembly without existance in a tree

Experimenter
Experimenter

Dear Tushar,

 

Thank you for the explanation.

 

Please have a look on step by step procedure, which is giving details of the problem I am facing.

 

1. PATTERN 4 -TUBE 05 TOWER-2 - IMAGE 1

 

Pattern 4 was showing 5 parts (TUBE 05 TOWER-2) except lower horizontal tube.( TUBE 05 TOWER-2.par:13)

 

2. PATTERN 4 -TUBE 05 TOWER-2 - IMAGE 2

 

The pattern 4 is showing TUBE 05 TOWER-2.par:13 after clicking on it.

 

3. PATTERN 4 -TUBE 05 TOWER-2 - IMAGE 3

 

Pattern 4 tree is showing 5 parts except TUBE 05 TOWER-2.par:13.

 

4.   PATTERN 4 -TUBE 05 TOWER-2 - IMAGE 4

 

The TUBE 05 TOWER-2.par:13 is still exist after deleting pattern 4.

 

5.  PATTERN 4 -TUBE 05 TOWER-2 - IMAGE 5

 

TUBE 05 TOWER-2.par:13  is not showing any option to delete it after right clicking on the part.

 

6. TUBE 01 -VERTICLE TUBE

 

When the length of Tube 01- Verticle tube is increased by 225mm then pattern becomes unsymmentric.

 

Hope above details are enough to fully understand your problem.

 

Please let me know if you need any further information.

 

Kind Regards,

 

Rahul Singh

Re: Part exist in a assembly without existance in a tree

Experimenter
Experimenter

Hi,

 

I have this exact problem, did you find a solution?

 

Dan