04-20-2016 11:04 AM
Dear Members,
I have an assembly in which I manually set the numbers of the parts. Now I want to use these part numbers as callouts on a draft. But whenever I try to create a linked ballon part number callout on the draft, it starts counting from 1. Whatever part is selected it starts from 1. I am using ST6.
04-20-2016 12:32 PM
This is the wrong forum to post that question as this is for those using the Free 2D Drafting product. Use the Solid Edge forum and you should get a good answer.
04-21-2016 12:17 PM - edited 04-21-2016 01:17 PM
I don't understand @KennyG's reply that this doesn't belong here. This is the Solid Edge Forum, isn't it?
Anyway, I'm not clear on what you mean by "manually set the numbers" but balloons typically reference an item number which is referenced by a parts list. To actually automatically show some value, as opposed to typing it, in a balloon which is not an item number you have to turn off "select item number" and use "select property text". Select property text will present a dialog in which you find the property to which you assigned part numbers. If that's what you did.
Maybe a screen shot of what you are trying to accomplish would help.
04-21-2016 12:17 PM
Without doing something like inserting the whole assembly or making a macro that goes back and adds a property to each item with the assembly item number you are stuck with manually changing it.
04-21-2016 02:38 PM
@bshand Somebody moved the post... It was in the 2D Drafting forum originally.
04-21-2016 03:11 PM
I shoulda figured.
04-22-2016 03:16 AM
Is this a case of setting the item numbers in the assembly model ?
If so you need to set your draft parts list to use them -
RMB on the Parts List > Properties > Options
The first checkbox at the top left 'Use Assembly Generated Item Numbers' needs to be checked.
04-22-2016 08:11 AM
Seems like he doesn't want item numbers. Anyway, I wonder, given that there has been no response from him, if he even knows the post was moved to a different forum?
04-22-2016 10:17 AM
04-22-2016 10:28 AM - edited 04-22-2016 10:32 AM
@nanan00, That's sort of true but is that what he was asking about? I'm not sure.
You can control if a new part shows up by using configurations or even (more rarely I assume) occurence properties.
Also if you pull in part views from the wizard from within the assembly structure they will track with the BOM. If you pull them in by browsing for them individually they will not track.