Cancel
Showing results for 
Search instead for 
Did you mean: 

Parts Library Pane view

Pioneer
Pioneer

Hi Folks,

 

Hopefully a quick one, nothing turned up in a forum search:

 

How do I go about adding/removing fields from the Parts Libray pane? We keep our file names aligned with the part numbers and descriptions in the comments property. I'd like to remove "Size" and "Type" and add "Comments". Alternatively, directions on adding any property text into the pane view would be immensely helpful.

 

parts_lib_fields.png



Solid Edge ST6 - Unmanaged
Win7 Pro - Dell Precision Xeon rig, 16Gb, Quadro M2000
3 REPLIES

Re: Parts Library Pane view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Don't think you can.

 

I have ER 7213308 created asking that the Parts Library Pane columns be selectable similar to Windows Explorer.

 

I also have ER 7213283 asking that the Solid Edge "Document Name Formula" be supported in the Parts Library Pane as well.

 

If you also want either or both, call your VAR/GTAC and ask to be appended to these ER's.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Parts Library Pane view

Pioneer
Pioneer

Will do, Ken. Thank you kindly sir.



Solid Edge ST6 - Unmanaged
Win7 Pro - Dell Precision Xeon rig, 16Gb, Quadro M2000

Re: Parts Library Pane view

Experimenter
Experimenter

Hey Ken, any feedback from Siemens on these ER's?

SteveD