Cancel
Showing results for 
Search instead for 
Did you mean: 

Parts List, Groups.

Creator
Creator

I want my Sub Assembly as the title and show its parts listed underneath.

Is this possible in Groups?

If so is there a tutorial showing how to use groups please?

7 REPLIES 7

Betreff: Parts List, Groups.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

maybe a fully strucuerde BOM with level baes pos numbers 20161102_1051.PNGdoes exactly what You are looking for?

 

regards
Wolfgang

Re: Parts List, Groups.

Honored Contributor
Honored Contributor

If you insert a sub assembly into a draft view, then create a parts list for that sub assembly, Then just label that sub assembly as a single line item in the main parts lists. I would try working that way if you don't want seporate drawings for the sub assembly.

 

One approach I have constered a few times.

Re: Parts List, Groups.

Phenom
Phenom

I think the problem here is that the option 'Show Top level Assembly in Parts List' only applies to the very top level - it doesn't apply to sub-assemblies.

So you can't show a sub-assembly as a line in the parts list with it's components also listed - one or the other, not both.

 

Maybe a good enhancement request.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Parts List, Groups.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are you asking if groups can behave similarly to assemblies in BOMs?

If so, no.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Parts List, Groups.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@beachcomber wrote:

I think the problem here is that the option 'Show Top level Assembly in Parts List' only applies to the very top level - it doesn't apply to sub-assemblies.

So you can't show a sub-assembly as a line in the parts list with it's components also listed - one or the other, not both.

 

Maybe a good enhancement request.


You can if you use "exploded list". Then possibly add "use level based item numbers" to help differentiate.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Parts List, Groups.

Creator
Creator
Thanks for your reply Beachcomber.

It would be very helpful for 3rd party checking of GA Assy's. When adding or removing assembled components (sub-assy's) to your generic Assy, which can end up very confusing.

Re: Parts List, Groups.

Creator
Creator
Thanks to all who replied!!!