Cancel
Showing results for 
Search instead for 
Did you mean: 

Parts List Views

Builder
Builder

Is there a way to have a parts list tied to multiple views? 

7 REPLIES 7

Re: Parts List Views

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

I am not expert at working with parts lists but on the few occasions I've had to do this I have just created parts lists for each view and then delete all but one of the lists.  The annotation callouts stay with the correct numbering.

 

Frank

Edinburgh University

Re: Parts List Views

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@SW wrote:

Is there a way to have a parts list tied to multiple views? 


Hi there,

 

I presume you are saying multiple views of the same Component, or Assembly.....? If so, then, Yes you can....just add baloons as required, making sure to activate the "Link To Parts List" option,  

 

You might like to review the information in this link for more...

http://www.soliddna.com/SEcommunity/page/articles.html/_/solid-edge-wiki/detail-drawing/partslists 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Parts List Views

Honored Contributor
Honored Contributor

Yes and No.

 

I do this by creating mutiple parts list, but only display one of them. This add the need to make sure both lists are configured the same.

 

Then I can have multiple views with a complete set of call out bubbles.

Re: Parts List Views

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

If I understand crystal clear what you want, you can do it.

 

You have to place a parts list what is tied to either drawing view and after this have to use Parts list command once again but toggle off "place Parts list" option and this will be tied to other view.

 

Here is a short video about this:

 

 

BR,

 

Imics
http://solidedgest.wordpress.com/

Re: Parts List Views

Honored Contributor
Honored Contributor

I wish that vid had english menus.

 

I have yet to figure out how to get item numbers to show up related to sheet metal flat patterns.

My BOM is is on a different sheet. The view is NOT assembly driven as it is a flat pattern.

 

Now: How do I get the item number for the flat pattern to show up? And yes, I want that item number to dynamically change as the BOM changes.

Note: it is imposible to get the item number to show up using annotation. They have religated all item numbering to that specific tool.

 

If it works at all, I assume the piece of the puzzle I'm missing is how to link the BOM from another tab to the sheet or bubble I'm trying to get the itme number into.

Re: Parts List Views;

Pioneer
Pioneer

Hi,

 

How to split quantities in part list in 3D assembly (using auto part list).In auto part list both components shows in single row quantity as 2. has both components  materials are different and we need to show it in two rows. (refer below snap for more information)

 Please let us know how to show two separate quantity of components in part list. 

 

Re: Parts List Views;

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello @Naveen10

 

Kindly stop adding new questions to existing discussions as you have been doing in several other instances.

This will create problems for you and others as explained in my PM.

 

Feel free to post new messages and you will find you will get plentiful replies within short time.

Thanks for your kind understanding.