Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Parts list position

Creator
Creator

Hey!

 

So everytime i need to place a parts list I have to manually go in to the properties and put in the value for where on the X and Y axis i want to place the list.

 

Is there any way for this to go smoother?

 

I use Solid Edge ST8 and i use the position X=235mm Y=59mm. I tried to save the settings but I still have the parts list attached to my mouse when I click on the view of the part.

 

Regards

6 REPLIES 6

Betreff: Parts list position

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

have a look onto the second sheet of BOM properties called position

 

There You will find in the upper left area of the prop table an option "use predefined origin for placement"

 

Click on that and SE will use the x,y coordinates in the lower right area for positioning!

 

 

regards
Wolfgang

Re: Parts list position

Phenom
Phenom

Hi here is a workaround!

 

X_Y.jpg

 

(X;Y) are the coordinates of lower right corner of the BOM when the macro "CAAP_Macro_PartsList_Replace.exe" is executed.

 

The templates have to be modified.

 

Here is the Youtube Video of CAAP "IN DUTCH!!!"
https://www.youtube.com/watch?v=mkj6tRMPfsg

 

To download the macro:
https://drive.google.com/file/d/0B3oRMVkY6HawU1V5RUJmek12d1k/edit?pli=1

 

Yasser

Re: Parts list position

Phenom
Phenom

By simply selecting the properties button for the parts list you can create a parts list insertion point for each draft sheet size you have to work with. Select the columns you want, the insertion point and the coordinates of the insertion point and anything else you want to capture and save each as a reconizable name. I have mine set to insert the parts list in the upper right-hand corner of A, B, C, & D sized sheets.

 

When I select the view, the arrow to the right of the properties button will display all of the saved arrangements you have and when you select one it places the parts list in the appropriate place. If later you change the sheet size, you simply select the parts list and grab the pulldown and change the selection to position the parts list correctly for the desired sheet size..

 

This parts list information is saved to a file called "draftlist.txt" and by default is located in the reports folder under your templates folder. You will want to make sure to move the file and/or folder when you upgrade to a newer version.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Parts list position

Phenom
Phenom

Hi Bob,

 

I changed the intersection point for A4 sheet with the upper corner of the parts list to:

x=210-5 ; y=297-5


The parts list sits in the appropiate coordinates and I saved this Settings under YD.

 

YD is now available from any other new DRAFT but the coordinates (X=205;y=292) are not.

 

Yasser

 

PartsList.jpg

 

Re: Parts list position

Genius
Genius

Are you certain you saved the configuration after entering the coordinates you need? I just tested this and it works fine for me, but I am on ST7. You must make all the settings and save it before you exit the window to place the parts list.

Bob Henry

Manager of Engineering - Highwall Miners
Caterpillar Global Mining LLC
Houston, PA

Re: Parts list position

Phenom
Phenom

Yes I did. But I am now working on ST5.

 

I will be able to try it on ST7 but in a few hours and let you know any updates...

 

Many thanks,

Yasser