Cancel
Showing results for 
Search instead for 
Did you mean: 

Parts misligned when .par drawings added to .asm drawing.

Experimenter
Experimenter

Having difficulties with components which are correctly oriented in .par drawing and when added to .asm drawing becoming misaligned. Any thoughts? See attachments.

 

Query_1.jpgDefault View in .asm drawingQuery_2.jpgFront view in .asm drawing

2 REPLIES 2

Re: Parts misligned when .par drawings added to .asm drawing.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @John_7,

 

One would normally use assembly relationships to position the parts in Assembly......alternatively, if they are in modelled in the correct location in model space, then hold the "Ctrl" key down while dragging your parts into the ASM file, and it will be placed as "Grounded".

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: Parts misligned when .par drawings added to .asm drawing.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @John_7

 

 

 

as already said by @SeanCresswell

 

You should not try to model the part in their ASM position, but with their production position and then You will place them in Your ASM, or even better, You will place them in many assemblies as the need to be placed there.

Or imagine, that one and the same part will be used several times in one assembly.

How will You model this?

 

regards
Wolfgang