Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Parts not showing with in Assembly

Experimenter
Experimenter

That did it. Thanks!

Highlighted

Re: Parts not showing with in Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@kevsdad01, I think I was least deserving of being assigned the solution but glad we could help.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Parts not showing with in Assembly

Honored Contributor
Honored Contributor

Since ST9, Surface models are not showing up. They added a new switch "Show contruction geometry when placing part that do not have a design body"

 

By adding that switch, any model that has surfaces and body's in it will not have the surfaces show up as a result.

 

Bad move from my perspective.