Cancel
Showing results for 
Search instead for 
Did you mean: 

Parts will not Drag to Parts and Assembly

N/A

I have a dozen or so... of parts to drag from Feature Library to .par and .asm and will not drag to appropriated drawings. What's missing?

Thanks
Crousie

3 REPLIES

Re: Parts will not Drag to Parts and Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Can you post a video or picture of what you are attempting?


Ken

Production: ST10 MP6
Testing: SE 2019

Re: Parts will not Drag to Parts and Assembly

N/A
This is the video for the part dragging, and what is the black circle?

http://screencast.com/t/JbpFD2LK

Re: Parts will not Drag to Parts and Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
It looks like you have a Part file open and that you are trying to drag files from the Feature Library tab into it.
You need to open an Assembly (ASM) file and then use the Part Library pane and drag the part into the Assembly.
It would also help with diagnosis if you include your entire Solid Edge window, not just a narrow slice...


Ken

Production: ST10 MP6
Testing: SE 2019