Cancel
Showing results for 
Search instead for 
Did you mean: 

Paste Function for Text

Genius
Genius

Is there any way to paste text into a text box without the formatting.  Ctrl+Shift+V does not seem to work.  Nothing worse than copying text off of a webpage and ending up with 30 inch tall text.

2 REPLIES 2
Highlighted

Re: Paste Function for Text

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I am not able to recreate the problem.

Copied the title of this post and pasted in a Textbox in Draft using Ctrl+Shift+V where it takes the default font Solid Edge ANSI with defualt height of .125 inch.

 

Re: Paste Function for Text

Genius
Genius

Weird.  I have an existing textbox that is Arial .187 text and when I paste into it the text is 36 inches tall.