Cancel
Showing results for 
Search instead for 
Did you mean: 

Pathfinder symbols/ icons

Legend
Legend

Does anyone know if there is  a key or "cheat sheet" showing all the possible pathfinder symbols? Every so often I come across one that I have no idea what it means. Or I can make a guess, but I would like to know for sure.

Using SE since V12, 2002
ST10 certified
6 REPLIES 6

Re: Pathfinder symbols/ icons

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

https://docs.plm.automation.siemens.com/data_services/resources/se/109/se_help/en_US/selfPacedExt/xi...

 

 The attached pdf says "ST6" so it may be a little out of date. Someone may have something newer.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Pathfinder symbols/ icons

Legend
Legend

That's the kind of thing I'm looking for but is doesn't have the icon I'm seeing. I think it indicates a synchronous hole is aligned with a feature on another part.

Using SE since V12, 2002
ST10 certified

Re: Pathfinder symbols/ icons

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I wouldn't think that would be a persistent relationship. Plus shouldn't it just show in "Relationships"?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Pathfinder symbols/ icons

Gears Phenom Gears Phenom
Gears Phenom

search SE help for "Legend"  this is used when SE help shows icons and meaning.

 

can you screen shot your icon in question ...

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7
Highlighted

Re: Pathfinder symbols/ icons

Legend
Legend
I figured it out after using Matt's search suggestion.

"Floating feature origin occurs when the face the feature was originally placed on no longer exists. To fix this, right-click the feature origin, and then click Reposition Feature to define a new face for the feature."

Except I tried this and I don't get any option like that when I click on the blue arrow or anything else I can find. I didn't make the part so I'll ask the guy who did how he made it. Anyway it doesn't seem to hurt anything.
Using SE since V12, 2002
ST10 certified

Re: Pathfinder symbols/ icons

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Right click on the hole in Path Finder and select "Show Feature Origin".

Now edit the hole by clicking the Edit definition handle(the leader).

While still in the edit mode, right-click on the big blue arrow and select "Position Feature".

Select the plane the hole origin shold be on.

 

 

LMGi
www.TLMGi.com